Part Number: TPS548D22 Hi team,
My customer is designing a system power supply based on TPS548D22, and have below requirement, please help to give your professional advice.
Vin=12V, Vout=5V, Iout_max=30A, Iout_ripple<200mV. Now there are two inductor…
Part Number: TPS548D22 Hi expert,
Do you have TPS548D22 short circuit test waveform can share as a reference?
What customer measured seems like OCP behavior. We expect Vo shall drop to 0 right away. Although they used E-load but they use multiple…
Part Number: TPS548D22 Hi:
According to the TPS548D22 datasheet, VBP is 2.93V in the page6. However, the BP LDO output voltage is 5.07V. Why is the discription different?
Thanks!
Jiajun
Part Number: TPS548D22 Other Parts Discussed in Thread: TPS548D21 We have an existing design using TPS548D22 with pin 37 connected to gnd via a 1000pF cap.
This is a mature design and seems to have no issues, though I see from some of the posts
that…
Part Number: TPS548D22
Hi,
I am implementing Vout = 0.675 Iout= 27A with feedback resistors on TPS548D22 evaluation board. I have set Vref (VSEL) to 0.5996V to provide the desired output voltage, as shown in the schematic below.
To limit the current…
Part Number: TPS548D22 Hi,
In the TPS548D22RVFR buck converter, We are using the output voltage set by VSEL(pin number 33) pin of TPS548D22RVFR, As per the datasheet VOSNS, RSP connected to the output and RSN connected to Load return,
We have simulated…
Part Number: TPS548D22 Hi team,
In TPS548D22, we suggest in the schematic checklist to connect a 1nF capacitor in parallel between the RSP and RSN pins.
What is the function of this capacitor? Are there any requirements or suggestions for its placement…
Part Number: TPS548D22 Hi Team,
When I am reading about OVP delay, the table below indicates the delay is 1us for OVP delay 100mV OD
Does it mean that when FB voltage is 120% above the reference, it needs to stay at 120%VREF+100mV for 1us to trigger…