Part Number: TPS548D26 Other Parts Discussed in Thread: TPS548C26 , I would like to use the TPS548D26 to power an FPGA (with GND sense and VCC sense). Voltage 0.8V, current max.15A. VIN is 4.5V..16V. This component is not supported in the Web Designer…
Part Number: TPS548D26 hello, I'm interested in using the TPS548D26, but there doesn't appear to be any simulation models. Does anyone know if there is a PSPICE model for a similar product? thanks
Part Number: TPS548D26 Tool/software: Hi,
Could you recommend proper device for AVS control by AVS_VDDFB of 98DX8572?
input: 12V, output:0.98V, 40A
Thanks.
Part Number: TPS546D24A Other Parts Discussed in Thread: TPS548A28 , TPS548D26 Tool/software: dears,
How to calculate the RL Model parameters of TPS548D26 &TPS548A28 ?
seems TPS548D26 has no SIMPLIS and Pspice model on the webpage.
thank you!
Part Number: TPS548D26
Tool/software:
In the Figure 6-2 of the datasheet for using external VCC bias, it suggests to tie VCC and AVIN pins together and then connects to VDRV via a 1ohm resistor. But in Figure 7-1, it shows AVIN ties to VDRV pin together…
Part Number: TPS548D26 Other Parts Discussed in Thread: CSD95373BQ5M , TPS543C20A Hi team,
My customer's Design condition:
Vin=12V, Vout1=3.3V (45A) ,Vout2=5V(30A) , analog solution.
I find ne TPS548D26 is suitable for 5V/30A rating.
But seems…
Part Number: TPS543C20 Other Parts Discussed in Thread: TPS548B22 , , TPS546B25 , TPS546E25 , TPS548D26 Tool/software: Dear Team,
It is found that the part TPS543C20RVFT has Lead over threshold. Please confirm if this is true and provide alternate part…
Hello Jimmy,
You are correct, there a 35A version of the 8C26. It up in the web and can get samples.
https://www.ti.com/product/TPS548D26
It depends what you care about, the 8D26 has smaller package.
Thanks
Tahar
Hello Kaviyasaran,
Another similar device for your parameters would be the TPS546D24A, however some differences would be that it operates on current mode control, is a different package type, and comes in a different package size. I have attached…