Part Number: TPS55010 Tool/software: I am using the TPS55010 to create an isolated PSU with 5V in and 7V out. I used the WEBENCH tool to create the design and I copied that to my PCB.
I built four PCBs and they all worked fine.
The next three PCBs…
Part Number: TPS55010
Hello, I'm looking to develop an isolated DC-DC with input of 3.3V and output of 12V with a maximum output current of 50 mA. The main consideration of this is low standby current drawn from input without any load on output - less…
Part Number: TPS55010 Hi,team,
My customer asked a question, please help answer it, thank you.
GB 9706.1 General Requirements for Basic Safety and Basic Performance of Medical Electrical Equipment
This standard requires that the input Vin shall…
Part Number: TPS55010 Hi,
We are currently planning to use the TPS55010RTER for generating 5V at Fsw=100kHz.
As per the datasheet, the resistance to be connected to the RT/CLK pin should be within the range of 1070kΩ to 42.2kΩ.
I have two questions…
Part Number: TPS55010 Hello,
My customer is looking at using this part for the following use case:
VIN = 3.6V
VOUT = 5.0V
typical outputs current 10's of mAs, but current spikes as high as 150mA.
They really like that the TPS55010 can be…
Part Number: TPS55010 hello, it is not new question, but supplement to my related question (unfortunatelly my previous qestion has been locked). I have design small transformer for 2x5V output voltage. I have used core with nominal AL=1200 [nH/Ts2] (core…
Part Number: TPS55010 Hello, I was trying to implement the TPS55010 reference design for a 3V3 to 5V supply with 50mA. Instead of the Würth transformer I used this one from CoilCraft: https://www.coilcraft.com/getmedia/92e0bb88-6d52-4797-af95-389405bc76a8…
Part Number: TPS55010 Hello TI experts,
My customer wants to isolate power lines, 5V/10mA.
and they want to minimum size for PCB.
I think that TPS55010 is the best part for them, but I cannot expect the size of transformer, even WEBENCH does not…