Part Number: TPS55010 Hi, This is Jay, TI sales.
I need your help to figure out if we have an ISO power module with 5V&6W output which is used to support 9 ISO CAN FD ISO1044BDR power supply .
And our customer is considering an competitor VRB0505ZP-6WR3…
Part Number: TPS55010 hello, it is not new question, but supplement to my related question (unfortunatelly my previous qestion has been locked). I have design small transformer for 2x5V output voltage. I have used core with nominal AL=1200 [nH/Ts2] (core…
Part Number: TPS55010 Anyone got a suggested alternative to the TPS55010? Doesn't need to be the same pinout, but maybe around same size ... 3mm square with integrated FETs. Looks like there will be no more of these until at least a year from now…
Part Number: TPS55010 Hi,
My customer need assistance.
https://www.ti.com/lit/ds/symlink/tps55010.pdf
On page 17, Table 1, 3.3 V to 3.3 V at 0.3 A, the RHS is 8.25 kΩ, RT is 511 kΩ.
While I use Webench to make a design:
https://webench.ti.com…
Part Number: TPS55010 Hello, I need 2 power supply: one with +-5V output and current less than 10mA and second for +-35V and current less than 10mA. I do not want use WE transformer, because for turn ratio 1:8:8, output voltage is too low (for +-35V) or…
Part Number: TPS55010 Hi, My customer is evaluating TPS55010, but he observed voltage drop on the PH side of L on one of three boards, because switching is stopped. You can see the following waveform. Could you please let us know the reason?
He said…
Part Number: TPS55010 Dear TI team: My customer used TPS55010 for 5V to 5V isolate application, they found TPS55010 heat up when there is no load, please help to check what is the problem? Thanks!
Is it because IC thermo pad is not connected to the…
Part Number: TPS55010 Hi, team.
i've been asked by Customer as below.
is TPS55010 feasible below customer requirement ?
temp range:0~100℃
load :0~180mA
output voltage :±5%
Input 5V
output:9V
what if customer does feedback from 2ndary , will…
Part Number: TPS55010 Hi Expert,
The customer configure the TPS55010 to Fly-buck,but see the high voltage stress at PH pin during the secondary winding short testing.
Seems there is no internal low side Mosfet current limiter of TPS55010.
Pls advice whether…
Part Number: TPS55010 Other Parts Discussed in Thread: LM25018 Hi everyone,
I have some questions as follows , thanks.
Q1 : IC is TPS55010 , what value is this I-HSCL ?
Q2 : Whether below calculate can used with above calculate portion ?
LM25018 …