Looks like LM5118 or LM25118 are the closest choices. They are not synchronous however. There is also an integrated synchronous solution, TPS55065-Q1. Output current is limited since the FETs are internal.
Adrian,
You are wanting to know this information about the TPS55065-Q1 correct? For future reference please post all questions about Q1 parts in the Automotive forum .
In any case, I will get back to you with the answers to your questions.
Other Parts Discussed in Thread: TPS55065-Q1 I am looking for characterization data on the Vg current limiting function. There are no examples in the data sheet or EVM.
Current limit delay is not given anywhere.
When Vg is overloaded while under steady…
Other Parts Discussed in Thread: TPIC74100-Q1 Hi All,
The TPS55065 switch-mode regulator does not start at V(driver) less than 5 V .
Once it started it can regulate 5V with input down to 1.5V
Unfortunatelly it is not an option for buck-boost requlator,…
Other Parts Discussed in Thread: TPS55065-Q1 , TPIC74100-Q1 We can see the waveform of Input Voltage Excursions of Figure 16 of TPIC74100-Q1, and Figure 15 of TPS55065-Q1. Are there any spec. or standard for Low-Crank Conditions?
and, please let me know…
Other Parts Discussed in Thread: TPS62050 , TPS61175 , TPS55065-Q1 , TPS61030 Looking for clarification on subject '800mA Synchronus Step-down Converter'.
I'm assuming, given that this is a switching DC/DC regulator, that (generally) the input voltage…