Part Number: TPS55165-Q1 Other Parts Discussed in Thread: LM51581 Hi Team,
Can you help clarify the question below?:
There are three fixed voltage supplying (5V(5%), 12V(5%) and 24V(5%)) into the customer board, and the output voltage is 5.1V(2%). There…
Part Number: TPS55165-Q1 Other Parts Discussed in Thread: TPS55165Q1-EVM Hi,
Our TPS55165-Q1 design works well but if we drive PS high and leave it for a few days in low-power mode we sometimes come back to a damaged part which outputs 0V. The load on…
Part Number: TPS55165-Q1 We use TPS55165 as a 12V voltage power supply with input voltage range 6-32V. Output voltage characteristics does not follow the datasheet data provided.
PCB rouding is in accordance to the datasheet recomendation.
There is input…
Part Number: TPS55165-Q1 Hi Team,
There is a good new that Customer is searching TI solution
The spec is following
*Vin=6~16V
*Vout = 5V ~12V
*Iout>1A
*AEC-Q100
*need enable
>>>Please suggest a best solution ,THX
Part Number: TPS55165-Q1 Hello,
My customer wants TI review of their TPS55165-Q1 circuit design.
Could you please review the following circuit design?
- VIN = 15.6V ~ 10.7V, VOUT = fixed 12V
Thanks,
JH
Part Number: TPS55165-Q1 Hi team,
Could you give me an efficiency plot below 0.1A for both normal PWM mode and Low Power PFM (PS=High) mode?
I need to improve low power efficiency and considering to use PS.
regards,
Part Number: TPS55165-Q1 Hi team,
Could you advise how does the device handle over current or output short circuit condition while in Low Power mode (PS=High) condition?
In the datasheet it seems over current protection function is disabled if PS=High…
Part Number: TPS55165-Q1 Hi Team,
I 'm designing the Buck-Boost with TPS55165. Vin:10-36V , Vout:12V , Iout: 400mA.
I analyzed the demoboard TPS55165-EVM.
I ask you if the input capacitors and otuput capacitors instead of 10uF 50V (2xCin and 2xCout…
Part Number: TPS55165-Q1 I am having stability issues with TPS55165-Q1.
Here is the schematic:
And this is how the layout look like:
The problem is seen when input voltage is around 11V and higher.
When input is around 11V the output is varying between…
Part Number: TPS55165-Q1 Hi,
I'm designing a buck-boost converter and in the datasheet ( https://www.ti.com/lit/ds/symlink/tps55165-q1.pdf?HQS=dis-mous-null-mousermode-dsf-pf-null-wwe&DCM=yes&ref_url=https%3A%2F%2Fwww.mouser.es%2F&distId=26…