Part Number: TPS552852 Other Parts Discussed in Thread: TPS63820 , TPS55285 Hi,
We would like to know is there have small size buck-boost solution for Vin (operation>9V),
Vin = 3~6V, Vout= 4V, Isw~4~5A.
Customer study for IOT device need small package…
Part Number: TPS552852 Other Parts Discussed in Thread: TPS55285 ,
Hello I'm Jaeho
I have some question, Check the below
Please let me know the tolerance range of ILIM pins
If the ILIM pin is designed with 100Kohm resistance, the Limit Current…
Part Number: TPS25730 Other Parts Discussed in Thread: TPS552852 , Hello I'm Jaeho Choi
I have some Question
Plz Check the Below
I am design a PD circuit with TPS552852 and TPS25730D.
I would like to control FAULT_IN of TPS25730D according to…
Part Number: TPS63805 Other Parts Discussed in Thread: TPS63060 , TPS55285 , TPS552852 i might be using 3 different batteries with 3 different input voltage and i want to select one most efficient regulator for 3 different VIN. the VIN are:
1) 6V
…
Hi Jaeho
Thank you for reaching out. May I know what is the application here? What is your target fsw? What is the Vin/Vout/Iout?
TPS552852 cannot set switching frequency without I2C. Changing the resistor value will not change switching frequency…
Hi Mulin,
Thanks for the suggestion.
Between the TPS55285 and TPS552852, is there any significant variation in efficiency?
Also, does the device support a pass-through mode or 100% duty cycle operation? When the input voltage is equal to the output…
Hello Mulin,
Thank you for the response. The application is to use the part as 12V output Buck Boost converter for supplying a DC Fan, with input voltage ranging from 6V to 22V.
If I understood you correctly,
1. I can use the part without I2C, only…
Hi Jaeho,
Thank you for reaching out. Same as last thread, do you have I2C in your system?
We have TPS552852 without I2C control, and the output current can be adjusted with resistor.
JAEHO CHOI said: If I don't set the Register, will the Output…