Part Number: TPS55288-Q1 Hi Team,
We are using MOSFET circuit to enable TPS55288-Q1, We are using low VGS throuslod voltage MOSFET(part number :UM6K34NTCN)
Below input deatils for voltage
Gate pin voltage (REG_SW_SEL_EN) : 1.8V
VBAT_IN_CON Voltage…
Part Number: TPS55288-Q1 I would like to use it for below application.
1) input : 12V~14V.
2) output: can be adjusted by I2C, 1V~20V.
2.1) voltage profile: 12V -> 1V, stay 50ms, -> back to 12V
2.2) voltage profile : 12V -> 20V, stay 1s -> back…
Part Number: TPS55288-Q1 Hi Team,
We are utilizing the TPS55288-Q1 IC in a buck-boost configuration within our design. When applying a 12V input, the output successfully regulates at 12V or 6V (buck mode). However, when configured for an 18V output…
Part Number: TPS55288-Q1 Other Parts Discussed in Thread: TPS55289-Q1 Hi,
Currently we are designing the Qi 2.2 25W In-car wireless charger. Can I use TPS55288-Q1 as the buck boost stage of Qi 2.2 25W Wireless power transmitter.
Part Number: TPS55288-Q1 For my application, the input power is 12V, output is 2~20V which could be adjusted by MCU, max output current is 8A, the switch frequency is 400KHz.
If I calculate the loop stablity part for pin COMP, I will get different value…
Part Number: TPS55288-Q1 Other Parts Discussed in Thread: CSD18543Q3A Input voltage: 26V to 6V
Output voltage: 12V
Max current: 3A
EN/UVLO, done with voltage divider
Generated from the webbench designer.
The issue i'm having is that…
Part Number: TPS55288-Q1 Hi Mulin,
Hi Mulin,
Regarding the schematic review for this IC,
We do not have availability for the IPZ40N04S5L3R6ATMA1 part, so we are replacing it with the IPZ40N04S5L2R8ATMA1. Please review and let us know your feedback…
Part Number: TPS55288 Tool/software: Hi team,
Customer wants to use TPS55288-Q1 for non-auto application due to some reason.
Could you please list all differences?
Best regards,
Hayashi
Part Number: TPS55288-Q1 Other Parts Discussed in Thread: TPS55288 , TPS552882 , TPS61299 Tool/software: Hello, We are going to use TPS55288-Q1 for 3.3V and 5V regulators from an input power supply between 2.8V and 5V, our Questions are: 1- Is TPS55288…
Part Number: TPS55288-Q1 Other Parts Discussed in Thread: TPS26743E-Q1 , USB2ANY , TPS55288 Tool/software: Hi,
Can I talk with the TPS55288-Q1 via I2C without an input at Vin? The datasheet for the part and the evaluation board show that an external…