Part Number: TPS552882-Q1 Other Parts Discussed in Thread: TPS552882
Tool/software:
Hi, TI expert
The customer configured a circuit with TPS552882-Q1 and wants to check whether the output voltage ripple is at an appropriate level.
Below is the…
Part Number: TPS552882-Q1 Hi Team,
We are working pin FMA for the project. May you help confirm below table?
Our safety goal is that the Vout needs to be stable.
Pin name
Open-circuited effect
Safety goal
Detection
…
Part Number: TPS552882 Other Parts Discussed in Thread: TPS55288 Hi,
Product A:
I thought I could use the TPS552882 to drive a laser with constant current, however the current limit range are too unstable and not suitable as I require an adjustable…
Part Number: TPS25751 Other Parts Discussed in Thread: TPS552882 , , TPS65987D , TPS55288 , TPS65987 , TPD4S201
Hello,
I would like to check with you what might be a problem with my design. In my opinion, soldering look good without cold joints. I…
Part Number: TPS552882
Tool/software:
Hi Teams,
Can the TPS552882 support the following input and output conditions? Vin 9~36V, Vout 12V, Iout 8A.
I tried simulating it using WEBENCH but couldn't get any results, thanks.
Otherwise, I found…
Part Number: TPS552882-Q1 Hi Team,
I would like to check if there is pull low resistor on MOSFET source node?
It looks like that only Rds(on) contribute the output L voltage, correct?
Roy
Part Number: TPS552882 Hi! On our EVM, TPS552882 Is used as the class H buck boost.
what would your suggestion be to supply PVDD a design which will be ~5W output , 25W max? Speaker resistance about 3Ohm
Vin would be 1s li-ion battery. Curious if…
Part Number: TPS552882 Other Parts Discussed in Thread: TPS55288 , TPS55289 , TPS552892 Tool/software: Hello, experts
We are designing a power station using TPS552882 and made several sample products.
During sample testing, we found 2 major problems…