Part Number: TPS552882-Q1 Hi, TI support team
What is the difference between TPS552882QRPMRQ1 and TPS552882QWRPMRQ1.
This is the inquiry for 'W' suffix.
Thanks.
Regards,
MJ
Part Number: TPS552882-Q1 Hi Experts,
on the website the max. output current for the device is mentioned to be 6.35A. What determines this current limit/capability? I did not find an explanation in the datasheet.
BR Simon
Hi Chul,
Thank you for reaching out on E2E.
1. We don't have such a WCA model for TPS552882-Q1.
2. May I know what kind of worst case analysis that you want to run? loop stability or steady state ripple?
The TPS552882-Q1 Pspice model is quite…
Part Number: TPS552882-Q1 ALL HI!
I choose to use tps552882-q1 to design the circuit. The input voltage is 8V ~ 36V and the output voltage is 12V. What is the maximum output current of tps552882-q1? If I use the design software on TI's official website…
Part Number: TPS552882-Q1 I am trying to drive the TPS552882-Q1 with a power supply of 12 to 28V and a battery of 2.8 to 4.2V. If I choose a MOSFET that can be driven by the voltage of the battery, the VGS rating will be 12V. Even if I look for it, if…
Part Number: TPS552882-Q1
ALL HI!
At present, tps552882-q1 is used for circuit design, with input of 8 ~ 36V and output of 12V / 3a. If the output is short circuited, tps552882-q1 can realize constant current 3A control? As shown in the figure below…
Part Number: TPS552882-Q1 Hi
My customer application condition as below, can you help recommend the inductor spec for below conditions ? thanks!
Vin = 5.5 V ~ 19 V
Vout = 9.2V, 5A
Switching frequency = 400KHz
Part Number: TPS552882-Q1 Other Parts Discussed in Thread: TPS552882 , TPS55288 , , TPS55288-Q1 Hi, I have a schematic based on a webench solution which I have modified slightly and I just want to check if everything looks ok. It is for 6-36V input with…
Part Number: TPS552882-Q1 Other Parts Discussed in Thread: TPS55288 I want to know why the switching frequency drops to half when in buck-boost mode on TPS55288. The switching frequency is halved when the input and output are 14V each, as shown below…
Part Number: TPS552882-Q1 Team,
My customer is asking:
There are two land patterns available for TPS552882QRPMRQ1 this part,
Which one need to be considered for our land patterns creation?
Also, standard land patterns is enough for this package…