Part Number: TPS55288EVM-045 Hi Team,
I have a question about TPS55288EVM board. The Vout will keep enable status when I change the value 0x03 to 0x00 at Reg[0x04h].
But when I TPS55288EVM_issue_E2E.xlsx , Vout will disable. The test information as attached…
Part Number: TPS55288EVM-045 Other Parts Discussed in Thread: TPS55288 , , TPS552882 Hello Team,
I am designing a USB PD Type A and Type C Wall charger and have shortlisted on TPS55288 for the DC/DC buck boost. below is my requirement -
Vin - 2.7 - 24V
…
Part Number: TPS55288EVM-045 Hi Team,
I have two questions about using TPS55288EVM-045.
1. When I removed 220uF Cout and I used GUI to set Vout = 6V or above, I could hear noisy on the board. (no load) Do you have idea why this noise occur?
2. Do we…
Part Number: TPS55288EVM-045 Other Parts Discussed in Thread: USB2ANY , TPS55288 , , TPS55288-EVM-GUI I have a new TPS55288 EVM board, and a new USB2ANY. I have the program up to work with the TPS55288, and the GUI Composer has been loaded. However the…
Part Number: TPS55288 Hello,
I have a question about the TPS55288 IC.
I have designed and made a schematic and PCB with the exact same components as the TPS55288EVM-045 Evaluation Board, and placed them on a much smaller PCB (about 25mm x 30mm) and I…
Part Number: TPS55288 Other Parts Discussed in Thread: USB2ANY Hi team,
We tried to connect our TPS55288EVM-045 but GUI always shows Hardware not connected. Failed to connect.
I already followed user guide's instructions, so currently I don't know what…
Part Number: TPS55288 Other Parts Discussed in Thread: , CSD18531Q5A
Hi TI guys.
I'm coming from company from Slovenia and I'm a firmware and hardware developer.
Our goal is to make a device which is capable of continuously supplying 100W from…