Part Number: TPS55330 Dear Sir/Madam,
I am using right now TPS55330(boost ) converter to convert +15V to +20v without load we are getting correct +20V which is expected , But when we apply load current 60mA then we are getting constant current (CC…
Part Number: TPS55330
Tool/software:
Hi team
I buil the circuit with the SEPIC configuration by TPS55330.
Ripple noise increases after loading ,and increases as the load increases
0.5A
1A
The burrs that appear should be generated on the…
Part Number: TPS55330 Other Parts Discussed in Thread: TPS55340 Hi Sir,
My customer using TPS55330 now but the lead time is issue.
Do you have comments for alternative parts with good LT solutions? only condition is need p2p with TPS55330.
This…
Part Number: TPS55330 Hi I got a problem Calculate according to the formula Input 12V, require output 16V, circuit as picture But the output is 19V, no matter if R175 is 120K or 100K Where is the problem? Thank you
1.229V x (R175/R177 +1)
Part Number: TPS55330 Hi, Team
this is MASA.
could you answer for me ?
1.can customer let IC's thermal pad opened ?
->will IC be able to work properly if there is no soldering at thermal pad flip side of IC?
2.can customer let IC's QFN soldering…
Part Number: TPS55330 Other Parts Discussed in Thread: TPS55340 , TPS61178 Hi gents,
I'm using the TPS55330 on my design to generate 15V from a 3 to 4.2V input.
Is there a way to calculate the maximum output current that my design can provide? on…
Part Number: TPS55330 Other Parts Discussed in Thread: TPS62130 , , TPS55340 I have a TPS55330 boost supply feeding the input of a TPS62130 buck supply. This combination is unstable. The output of one or both of the supplies becomes shorted to GND during…