Part Number: TPS55340 Other Parts Discussed in Thread: TPS55330 Hello,
My customer is facing delivery issue of TPS55330RTER.Looking at TPS55340 datasheet, TPS55340RTER looks the same package, WQFN(16), and pin assignment. TPS55340 Vin range is wider…
Part Number: TPS55330 Other Parts Discussed in Thread: TPS55340 , TPS61178 Hi gents,
I'm using the TPS55330 on my design to generate 15V from a 3 to 4.2V input.
Is there a way to calculate the maximum output current that my design can provide? on…
Part Number: TPS55330 Hi team,
please help to
1. review the following schematic
2. confirm that the inductor is ok.
3. please let me know if their inductor is overkill for their design.
VIN= 12V
VOUT= 20.7V
IOUT= 2A
INDUCTOR = SDR1806…
Hello Jasper, Thanks for your support. I indeed need a sepic topology, however I am not very familiar with such topology and I would like to have a template or reference schematic for this TPS55330 IC. Is there any available? I am surprised that there…
Part Number: TPS55330 HI!
I want to oder tps55330 parts by sample proecess.
but, can't access website. there is comment "sample problems"
how do I solve that problems.?
thanks.
Part Number: TPS55330 Hi
I got the request from my customer.
They would like to get the open short test data of TPS55330.
Do you have these data?
Best regards,
Yokota
Part Number: TPS55330 Other Parts Discussed in Thread: TPS61089 , TPS61088 Dear ,
we used TPS5530,output current is loaded to 1.6A when the output voltage began to decline, the phenomenon of overcurrent protection, datasheet protection current as follows…
Part Number: TPS55330 Dear,
out client want to design TPS55330, and we try WEBNCH tool,
Vin:9V-14V ; output: 15V/0.5A ; it`s okay ; but Vin:9V~15V ; output:15V/0.5A it`s cannot print schematic.
it`s does not cannot meet?
If any suggestion, Please…
Part Number: TPS55330 Hi support team,
Will the output voltage change when switching from normal PWM to DCM at the light load?
Thanking you in advance, Takahashi Hirokazu