Part Number: TPS55340-Q1 Hi,
My simulation is throwing following errors :
Somebody please look into it and help me to resolve this issue. Please consider this query ASAP.
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS55340 Hi,
While simulating the PSpice model of TPS55340-Q1, the simulation is throwing this error " Trouble parsing initial condition value for node V(n006) ". This node is actually the SS port…
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS55340 , LM5157-Q1 Hi Expert,
We are trying to find some alternative solution for TPS55340-Q1 due to the shortage. May you check if we have P2P compatible one with TPS55340-Q1?
Thanks!
Ethan …
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS55340 Hi Team,
Could you help to publish or provide the package information of our TPS55340 WQFN RTE16?
There have detail info about our PWP14 package but no RTE16.
Hope for your feedback…
Part Number: TPS55340-Q1 Dear team,
Could you please help review below schematic? Thanks!
Application condition:
Input voltage range: 6v – 18v
Output voltage: 22v
Maximum output current: 1.4A
Allowable output voltage ripple: 2%Vout
Allowable transient…
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS55340 , TPS61088 , TPS61288 Hi,
I am going to add a boost regulator to generate 12V output from single cell battery (Vmin = 2.7V, Vmax = 4.2 (fully charged) ) and our current requirement is 2A…
Part Number: TPS55340-Q1 Hi, TI Support Team
Please review the circuit diagram and answer any questions regarding the attached materials.
- TPS55340QRTERQ1
TI DCDC Boost TPS55340QRTERQ1 Review Request_210929.xlsx
Thanks.
Regards,
MJ
Part Number: TPS55340-Q1 Hi,
Please let me know the effect on TPS55340-Q1 output voltage for below condition.
AGND Pin 6 is open, is AGND connected internally together with rest of other GND pins ?
Regards,
Bogdan
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS55340 Hi team,
I'm using TPS55340-Q1 in SEPIC topology.
TPS55340-Q1 has 2.9V minimum input voltage. I'm going to use some bulk capacitance (polymer or maybe EDLC) to withstand input voltage…
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS55340 Hi,
TPS55340 is used in SEPIC configuration and I need to estimate IC temperature.
Rds_on is presented in datasheet, so it's possible to calculate power dissipation when internal MOSFET…