Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS55340 Hi ,
Please let me know the effect on TPS55340-Q1 output voltage for below conditions.
SYNC Pin is open:
FB Pin is open:
FREQ Pin is open:
SS Pin is open:
COMP Pin is open…
Part Number: TPS55340-Q1 Hi, Team,
In our design excel, there have two formula to calculate the Ccomp, one of it is using the fp_mod, as followed:
But in our datasheet, it looks Ccomp is related with fz. Could you help clarify it? Thanks!
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS55340 , , TPS55332-Q1 Tool/software: WEBENCH® Design Tools Hi,
I was using Webench Power Designer to recommend a power supply for our requirements which are as follows:
Input: DC 3.2…
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS55340 We have a design that requires a high output capacitance and wanted to confirm the TPS55340-Q1 will be able to handle everything. We are looking for a 24V to 36V boost with maximum 2A…
Part Number: TPS55340-Q1 Hi team,
May i get your help to confirm how the equation 40 comes out on the datasheet of TPS55340-Q1(page 22), is there has any formula deduction for this equation?
Could you please kindly help to share some material which…
Part Number: TPS55340-Q1 Hi TI expert,
When setting the switching frequency higher than1.2 MHz, TI recommends using an external synchronous clock as the switching frequency to ensure that the pulse-skipping function works at a lightload.
Should I…
Part Number: TPS55340-Q1 Hello, I am using two TPS55340QRTERQ1 regulators to output 15V @ 1.5A and 28V @ 0.5A using 12V input in my boards. I using the EN (Enable Pin 3) function to control the regulator outputs. The regulator operates correctly during…
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS55340 , LM5157 Hi Sir,
(1)If the part can be used as buck boost application. (Vin varying from 9~36V, Vout=12V, Iout=?)
(2)At Vout 12V condition, what is its max Iout?
(3)Using SPEIC topology…
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS63020-Q1 , TPS55340 Hello, I wish to use the TPS55340-Q1 in sync with other supplies (TPS63020-Q1), which accepts a sync frequency of 2.4MHz +/- 200 kHz. The TP55340-Q1 would work for my application…
Part Number: TPS55340-Q1 Dear support team
Could you provide the frequency response data of the error amplifier of TPS55340-Q1?
I want to verify of stability of SEPIC circuit.
Regards
Tomohiro Nagasawa