Other Parts Discussed in Thread: TPS40211 , BQ24617 , TPS55330 , TPS55340 , TPS40210 , TPS55340EVM-017 Hi,
I need advise is it OK to put TPS40211 between BQ24617 output and system input? System needs to be supplied with 12V and 2A. BQ24617 has 12V adapter power…
Hi John
I recorded some measurements, the measurement points are always the same: Channel2 Diode D1(anode), Channel 4 Diode D1(cathode).
Scope settings: Channel 2 and channel4 coupling: AC
Old design without load:
Old design with load of ~70Ohm
The…
Other Parts Discussed in Thread: TPS55340 , TPS55330 Hi,
My customer has question about TPS55330 and TPS55340. Could you tell me about questoin?
[Question] My customer designed TPS55330 and TPS55340 under the following condition by WEBENCH.
Vin=3.6V to 4…
Hi Helen-san,
Thank you very much for your prompt reply and suggestion. I apologize for the delay in replying to you.
Design conditions are as follows. Device:TPS55340-Q1 Vin:5~16V - Maximum input voltage is 30V or more. - I chose the external…