Part Number: TPS55386EVM-363 The efficiency shown in the app note is measured independently for 3.3V and 5V by enabling both? Or one at a time by disabling other.
If I have to measure the efficiency of this converter can you please let me know the correct…
Part Number: TPS55386EVM-363 Other Parts Discussed in Thread: TPS62933 As per datasheet Vin max 28V but in EVM user manual mentioned upto max 13.2V.
As per my requirement is Input 24V
output 1 required to Max 18V
Output 2 Required to Max 3.3V can…
Dear Lucia,
1) I have connected the EN1 and EN2 directly to GND with no capacitor
2) I removed this capacitor
3) I am using the same compensation values
However, it is still delivering ponly 3.4V something.
To make sure my design is right…