Part Number: TPS560200-Q1
Hi
I aim to use the TPS560200-Q1 in design to get 3.3V max 400-450mA during peak Wifi TX, otherwise less then 100mA. My Vin will be 12V
This is my design, i have not yet done PCB layout.
I prefer to keep my BOM as universal…
Part Number: TPS560200 Hi team,
I have a question about the FB resistor.
My customer would like to avoid the pulse-skipping Eco-Mode, so they're considering to flow dummy load by reducing the FB resistance. How low can this device allow FB resistance…
Part Number: TPS560200 Hi
My customer want to know the switching frequency at Vout=5.0V.
Could you provide the curve at Vout=5.0V similar to the following graph?
Best Regards, Taki
Part Number: TPS560200-Q1 Hello,
my customer is currently working on a design with the TPS560200-Q1 and has a question.
Are there any care about with respect to the feedback loop and what is the minimum values of the required ESR for proper operation?
…
Part Number: TPS560200-Q1 Hi Team,
The customer is searching the DCDC solution for their Automotive application.
The specs is Vin=12V, output=3.3V/100mA.
There is a considerable noise which may generate inrush current/ voltage and damaged the board while…
Part Number: TPS560200 Other Parts Discussed in Thread: TPS560430 Is there any reason why the TPS56022900, or for that matter any similar buck converter part, cannot be used in the traditional inverting configuration, in which the 'normal' output is grounded…
Part Number: TPS560200 Other Parts Discussed in Thread: TPS561201 We are using TPS560200 to step-down 10V to 5V.
We have built the schematic following the guidelines given in the application circuit of the datasheet.
The generated 5V is fed to TLV1117LV33DCYR…
Part Number: TPS560200 Other Parts Discussed in Thread: TPS561208 , TLV62565
Hi team,
My customer wants to use TPS560200 in PWM mode not to affect the switching noise to other IC.
I understand TPS560200 enters the pulse skip mode when the integrated current…
Part Number: TPS560200 Hi, I am working on a project that requires me to step down from 12v- 14.4v 3.3A battery to 3.3v 0.5A in order to operate a STM32.
I drew an schematic regarding it but still have hard understanding on enable slot.
If i leave enable…
Part Number: TPS560200 Other Parts Discussed in Thread: TPS561201 , TPS561208 Hi TI Team,
We are using switcher ( TPS560200DBVR) in our project in this part maximum output current 0.5A, but we need >0.8A Max output current rating footprint and functionality…