Part Number: TPS560430 I am reporting a new problem that appeared during production on the TPS560430YQDBVRQ1 - HIZ56043Q1_LF system - the problem concerns barely visible markings that the AOI machine has trouble reading during inspection/vision test.…
Part Number: TPS560430 Hello,
We are studying TPS560430-Q2 in order to supply our Can Transeivers. A minimum SW frequency of 1.7 MHz is required; that is why the initial plan was to use the FPWM version, but after performing some calculations, we realized…
Part Number: TPS560430 Tool/software: Hello
I am atm having some trouble with the EMC tests. I have a system with a TPS560430 2.1Mhz switcher. And have some noise on both power in and SW out side.
What can I do? I have tryed with 10uH coil at…
Part Number: TPS560430-Q1 I am looking for the coefficient of thermal expansion (CTE) of part numbers LMR50410YFQDBVRQ1 & TPS560430YQDBVRQ1 in the SOT-23-6 package above and below its glass transition temperature.
Part Number: TPS560430 Hello,
I wonder if TPS560430 allows an output voltage greater than input voltage, f.e. if the circuit connected to the SMPS output will be powered by a debugger/flasher in production.
In the absolute maximum ratings of the…
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: TPS560430 Tool/software: HI Team,
Hope all is well.
My customer is Xingyu.
Currently they want to use this device for platform design, so they hope to have a standard schematic design that…
Part Number: TPS560430 Other Parts Discussed in Thread: LM5157 , LM5118 , TPS552872 Tool/software: Hello Every One,
I need design for above part having input range 7- 36vdc & output 15vdc on same input range with 150mA output current.
Part Number: TPS560430 Tool/software: To whom it may concern,
Hello, from the datasheet it's not clear for me if the FPWM version will or will not employ frequency foldback.
Section 8.3.4 Minimum ON-time, minimum OFF-time and frequency foldback does…
Part Number: TPS560430 Tool/software: HI,erery one,I have a issue about of the IC that is TPS560430XF(1.1MHz,PFM),below is light load,the out have a period output fluctuation,about 1ms,below is the out:
1.when access load,the o utput fluctuation is…