Part Number: TPS560430 Hi Team,
By application note, I know that TPS560430 can generate negative Vout. In application note, I have some questions need to confirm.
1. It is written here that the input voltage of the TPS560430 is greater than 4V, but I understand…
Part Number: TPS560430 Hi team,
My customer wants to use TPS560430 for negative voltage power supply.
The input is 4.5-9V, the output is -2.5V, and the output ripple is 5mv. How should I design it?
Hi Richard, As I requested early, now please add below query for the previous case. Requesting to provide Mosfet's Gate charge, LDO output voltage & Boot diode forward voltage drop for TPS560430-Q1. I hope a quick response. Regards, Vamsi
Part Number: TPS560430 Hi Experts,
A customer would want to know if the alternative automotive part TPS560430YFQDBVRQ1 (with available stocks) can be used as drop-in replacement without any changes to their existing design components.
I am aware from their…
Part Number: TPS560430 Hi team,
I want to doubel check if the AEC-Q100 qualified is the only difference between TPS560430Y and TPS560430YQ?
While go through I could not find any different spec, could I use the Q1 version to replace TPS560430Y directly? …
Part Number: TPS560430 Other Parts Discussed in Thread: TPS629210 , Our design uses a TPS560430XF part with Vin = 7.2V, and Vout = 3V3.
Our design requires a very low quiescent input current for very light loads (4uA), however we have measured a 4.5mA input…
Part Number: TPS560430 Dear Sir,
I am looking TPS560430 with 3.3V fix version.
It seems fix Vo is quite suitable for my MCU 3.3V
But my manager ask me to find the Vref need to be all positive or negative coefficients.
So we can capture the temp and calibrate…
Part Number: TPS560430-Q1 how to calculate the ripple current of Cout capacitor ripple current?
Vin:-
min = 6V Typ = 12V Max = 16V
L = 10uH; Cout = 10uF;
RFBT = 51k; RFBT = 22.1k
vout =3.3V
how to calculate ripple current of Cout capacitor?