Part Number: TPS560430-Q1 Tool/software: Hi Team,
My customer Meta System is testing the unencrypted model of TPS560430-Q1, but they get below error. Can you advise how to solve?
Also, they said they need long time to stabilize the output, do you have…
Part Number: TPS560430-Q1 Tool/software: Hi team,
I tested the bode plot on customer's board. It was strange.
I think it is because customer did not solder a wire on 50 ohm+. I had to link the test device to Vout pin.
Do you have a bode plot result…
Part Number: TPS560430-Q1 Tool/software: 1538.5V,600mA Reg.pdf I have attached a schematic design with the input voltage of 12V and output voltage as 1.5V with the current rating of 600mA. Can anyone please confirm the design is correct or if any changes…
Part Number: TPS560430-Q1 Hi,
can you let me know the failure mode to be consider for TPS560430-Q1.
Also what is failure mode distribution for the above IC.
Thanks and Regards,
Mangesh
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: TPS560430 Hi team,
I heard that your team currently doesn't have any data of CISPR25 like below. I'd like toc confirm it. If no, could you provide me some data that can be reference for EMI consideration…
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: TPS560430 Hi Team,
The TPS560430 has less output capability than LMR50410YQDBVRQ1 and the same switching frequency. Why is the output inductance twice as large as that of LMR50410YQDBVRQ1?
Thank…
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: TPS560430 Requesting to provide (Efficiency vs Load Current characteristics for 15V output), [High-side MOSFET ON-resistance and Low-side MOSFET ON-resistance at (TJ = 125 °C, VIN = 18-24 V range…