Part Number: TPS560430-Q1 how to calculate the ripple current of Cout capacitor ripple current?
Vin:-
min = 6V Typ = 12V Max = 16V
L = 10uH; Cout = 10uF;
RFBT = 51k; RFBT = 22.1k
vout =3.3V
how to calculate ripple current of Cout capacitor?
Part Number: TPS560430-Q1 Hi Team,
We have used TPS560430YFQDBVRQ1 in an automotive design.
The input operating voltage ranges from 7V to 16V. The typical voltage is 13.5V.
The required output current is ~500mA
Kindly review the following schematics and…
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: TEST2 Dear team,
There are two questions follow:
In the datasheet "8.3.2 Adjustable Output Voltage" part, resistor RFBT, RFBT in the range from 10 kΩ to 100 kΩ is recommended for most…
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: LMR43610-Q1 As per the Datasheet recommended operating conditions, VIN Max is 36V only. Can you please confirm if this IC can withstand the 40V Load dump pulse?
Part Number: TPS560430-Q1 Hello TI Team,
I am using the TPS5640 for generating 5V@200mA by 10V input voltage. Now I try to understand what happens, when the output is connected:
1) through a short to GND
2) through a short to supply voltage (say 16V…
Part Number: TPS560430-Q1 While doing the simulations for this buck converter tps560430y, encountered 2 problems :
1)When load resistor of 10 ohm is connected , not getting the required output voltage i.e 3.3 V
2)Also, when EN is grounded ,output is…
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: TPS560430 , Hello, I'm looking for spice model of this IC but I can't find it on the website, can you please assist me with this?
Best, Milos
Part Number: TPS560430-Q1 Hello, I would like to know the output voltage tolerance for TPS560430-Q1 buck converter IC.For eg.. 3.3 V +- 1%. Not able to find in the datasheet.
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: LMR16006Y-Q1 , , TPS560430 , LMR16006 Dear team,
My customer wants to use TPS560430-Q1 to replace LMR16006Y-Q1 with minimum change because the design has been fixed.
Change U1 from LMR16006 to TP…