Part Number: TPS560430 Other Parts Discussed in Thread: LM61495-Q1 , LM61440-Q1 , TPS552872-Q1 , TPS628503-Q1 Tool/software: Can you share the SIMPLIS model of the parts list below?
<parts list>
No.
DC/DC
1
LM25148QRGERQ1
2
LM61495-Q1
3
L…
Part Number: TPS560430-Q1 Hi team,
Could you tell me how much consumption current of PWM control is @ VEN = 3.3 V, VOUT = 5V, Iout = 0A?
Datasheet says just its PFM mode control device quiescent current. I am interested in PWM mode device (or TPS560430…
Part Number: TPS560430-Q1 hi Sir/Miss,
May I use 0.1% tolerance resistors for the Feedback path?
Why is it only 1% tolerance resistors are recommended?
0.1% resistors have lower TCR and TEF (total environment factors).
Part Number: TPS560430-Q1
Good day TI experts,
I am reading about TPS560430-Q1 PFM and FPWM version. I understand that PFM offers higher efficiency during light current loads (my application consumes low current about 220mA max).
But FPWM has low output…
Part Number: TPS560430-Q1 Hi,
I am using TPS560430YFQDBVRQ1 in one of my designs with 9V as its input and 5V as output. The total current consumption of the board without any code running is 8 mA. I bypassed TPS560430YFQDBVRQ1 regulator and directly provided…
Hi Marco,
The link in datasheet page 16 is not working,we will report this issue to concerned team.
Below is the procedure to create Webench design for device TPS560430YFQ.
Step 1: Kindly use device TPS560430-Q1 product folder link mentioned below to…
Part Number: TPS560430-Q1 Other Parts Discussed in Thread: TPS560430 , Hi,
we are aiming to use the TPS560430-Q1 (automotive raitng is required) to maintain a 5 V supply sourcing an output current of about 50 mA - 100 mA. The input voltage is between 5…
Part Number: TPS560430-Q1 From the application report "Loop Response Considerations in Peak Current Mode Buck Converter Design", the Gdi‘s expression from equation 2 simplified to equation 3, Gdi=Vin/s*L, the reason is "The internal loop compensation…
Part Number: TPS560430-Q1 Hi team,
If you have a EMI test result of TPS560430-Q1 without shield,
could you share it with me?
I see Figure 28 in snva886.pdf passes successfully. I would like to see the result without shield for this exact board and se…
Part Number: TPS560430-Q1 Hi expert,
I did't get a CAD drawing on TI.com, could you please let me know how can I get CAD file for below device?
TPS560430YQDBVRQ1
UCC27524A1QDGNRQ1
Thanks
Sheldon