Part Number: TPS561201 Other Parts Discussed in Thread: TPS54202H Hi expert,
Do we have P2P device of TPS651201, but with higher input voltage(more than 24V)?
Thanks!
Part Number: TPS561201 As per PCN 20210730004 .1, TI has made material change to TPS561201DDCR. Please provide updated material document which reflects changes mentioned in PCN.
Part Number: TPS561201 Other Parts Discussed in Thread: TPS562208 , We use tps561201dc in our design, but we can't get it at present. We have tps562208ddc in stock, but we only need 1A current. Can we use tps562208ddc instead of tps5612011ddc without repairing…
Part Number: TPS561201 Other Parts Discussed in Thread: TPS56339 , TPS563211 , TPS562211 TPS561201's current protection is to monitor the low-side FET drain to source voltage. However, if the overcurrent protection occurs during the high side on-time, OCP…
Part Number: TPS561201 Good evening to everyone,
i'm using this IC with this attached layout.
My SW node trace pass underneath the device.
Could be a problem for this IC during the operation?
My working parameters are:
- Vin min: 10V & - Vin…
Part Number: TPS561201 Tool/software: WEBENCH® Design Tools Hello
We make a RF Gate way
Power supply is 12 rail line and Solar panel + batteries .
we have RF 2.4 wifi Transmitter . 500mA peak (3.3V)
2x 915Mhz or 2x433Mhz 100mA peak (3.3V)
1 Mcu 8 mhz…
Part Number: TPS561201 Hi there,
I just read the datasheet of TPS56120x, it seems like TPS56120x has no OVP function.
I want to make sure if TPS56120x have OVP function or not.
Thanks
Part Number: TPS563201 Other Parts Discussed in Thread: TPS561201 Tool/software: I am currently using the TPS563201 buck converter for converting 12V to 3.3V, and we are utilizing a 2.2uH 7A rated inductor . Due to size constraints in our design, we are…
Part Number: TPS561201 Hi,
I am using TPS561201DDCR as in the attachment.
The design has glass and plastic cover. The design has pretty high failure rate when we do ESD test with 15KV gun. The Vin pin is shorted to GND.
Please advise if there is anything…
Part Number: TPS561201 Other Parts Discussed in Thread: TPS54202H Hi Team,
In Tps561201 the maximum output voltage which can be set is 7V maximum as per the datasheet.
This limitation in output voltage is coming from where?Is it due to topolgy of buck…