Part Number: TPS562202 Tool/software: Hi, Does this PSpice model work under non recommended values used on the inductor? For example with my steady state simulation, Vout : 5V from Vin: 7.3V Inductor used: 2.2uH, 140mOhms Feedback voltage divider resistors…
Part Number: TPS562202S Tool/software: Hi Sir,
I am experiencing an issue with the output voltage. The conditions are as follows:
Input is set to 12V
Output is set to 5V
Currently, the output remains at 5.6V. Could you please advise me on how to troubleshoot…
Part Number: TPS562202 Other Parts Discussed in Thread: TPS562207 , Tool/software: Hi, Please see my attached tested circuit below I currently have a very fast dynamic PWM load (~30kHz) which is causing a very large output voltage pk-pk ripple on the 5V…
Part Number: TPS562202 Other Parts Discussed in Thread: TPS562203 Tool/software: Hello experts,
In the datasheet of TPS562202, I found Vout decreases 25mV when Iout increases from 0.2 to 1.8A.
What is the main cause for this?
Regards,
Kento
Part Number: TPS562202 Other Parts Discussed in Thread: TPS62932 Why does the TPS562202 have an output voltage limit of 7V?
Usually buck regulators can go up to input voltage.
Is it because of the specified current (i.e. power dissipation limit)?
I only…
Part Number: TPS562202 Hello all. I'm trying to use two TPS562202 to step down a 12V input down to 5V at 1A and 3.3V at 1A. I'm looking to estimate input voltage ripple for my application, but I'm not seeing a formula on the datasheet anywhere. Is there…