Part Number: TPS562202S Other Parts Discussed in Thread: TPS562202 Hi,
I designed a 5V buck regulator using the TPS562202S IC, which I use to step down a 10 V input. I followed all the design guidelines for this first design, using the recommended component…
Other Parts Discussed in Thread: TPS562202 Dear Commnity,
I am trying to simulate the TPS562202 module in Pspice for TI with parametric analysis for feedback resistor tolerance of 1%.
I am getting below error while simulating.
Kindly let me know what could…
Part Number: TPS562202
Hello Sir,
I've been trying to use the "TPS562202 Buck Converter" to achieve a voltage output of 5V@0.5A from a Voltage input range of 10V to 17V. As shown in the image above, I had tried to do a PSpice simulation…
Part Number: TPS562202S Figure 9-11 in the datasheet shows Vout sinking very quickly after Enable is pulled low; is the low side FET on or off when enable is low?
The datasheet indicates the part won't be damaged if the SW pin voltage is greater than…
Part Number: TPS562202 Hello sir,
Good day.
I would like to know that for IC - TPS562202 switching regulator IC (BUCK IC) , What value need to select for 5V output.
In datasheet it mention, not installed for 1.2V(lower output.
Here, I'm attaching my…
Part Number: TPS562202S Other Parts Discussed in Thread: TPS562207S Hi, I'm using the TPS562202SDRLR in a new design. During my initial board bringup, I'm seeing some very strange behavior--I'm seeing 60-100mV ripple, which is much larger than the…
Part Number: TPS562202
Can someone help me understand the difference between the S and non-S versions of the TPS562202 device? They both have eco mode and the same efficiency curves.
John
Part Number: TPS562202 Hi Team,
As our new TPS562202/3202 device with SOT-563 package has the same pinout with MPS's MP165x which is widely used in our customers, customer wants to check if we can make the directly replacement on customer's board with…
Part Number: TPS562202S Can the Enable pin be tied directly to Vin? I have a new custom prototype board that has two blown TPS562202S chip on first power-up. Two other boards work fine. I used the WebBench design for both. Vin is ~+12V.