Part Number: TPS562202S Other Parts Discussed in Thread: TPS562207S Hi, I'm using the TPS562202SDRLR in a new design. During my initial board bringup, I'm seeing some very strange behavior--I'm seeing 60-100mV ripple, which is much larger than the…
Part Number: TPS562202 Hi Team,
As our new TPS562202/3202 device with SOT-563 package has the same pinout with MPS's MP165x which is widely used in our customers, customer wants to check if we can make the directly replacement on customer's board with…
Part Number: TPS562202S Can the Enable pin be tied directly to Vin? I have a new custom prototype board that has two blown TPS562202S chip on first power-up. Two other boards work fine. I used the WebBench design for both. Vin is ~+12V.
Part Number: TPS562202
Can someone help me understand the difference between the S and non-S versions of the TPS562202 device? They both have eco mode and the same efficiency curves.
John
Hi Kygo
Does customer want to use an automotive device? TPS54232 is not the automotive solution. If customer prefer an automotive solution, I would recommend TPS629210-Q1. Otherwise, I would recommend TPS562202/7.
Is there any special concern here? Like…
Part Number: TPS563202 Other Parts Discussed in Thread: TPS562202 , I have a design where the TPS563202 (and possible alternate TPS562202) is configured to output 5V, and I want it to work with an input voltage range of about 4.5V to 16V. I would like to know…
Hi Miranda Gu,
Thank you for the reply.
I also tried simulating TPS562202 and able to get the results, but I am facing some issue in parametric analysis,
I am simulating TPS562202 circuit with feedback resistor tolerance 1%, below is the result what I…
Part Number: TPS54JA20 Other Parts Discussed in Thread: TPS562202 , TINA-TI ,
After generating my design for the TPS54JA20RWWR, I was so glad to see that you now offer the export of the schematic and layout to the popular tools. Upon attempting to export…
Marco,
I would take a look at TPS562202, It doesn't have the ability to use softstart or mode selection, but I would expect it to behave similar to TPS562211.
Thanks,
Joseph