Part Number: TPS562207 Dear Team,
I am looking for VDS spec of TPS562207 internal MOSFET.
I only find low side FET spec(SW) from datasheet. Could you share HS MOFET VDS spec with me?
Thanks,
Ben
Part Number: TPS562207 Dear Power management team
I’m trying to perform the following simulation:
Im having 2 main problems with it,
When you look at the voltage divider at the right you will see that the division is very odd, the voltage…
Part Number: TPS562207 I have a new prototype design with 3 samples built.
The design is required to produce 5V output from this buck converter and I have fitted the following components:
R1=47k, R2=240k, 0.1u Feed forward cap,10u input cap, 22u output…
Part Number: TPS562207S
I would like to know what happen if the TPS562207S buck converter exceeds the maximum duty cycle (80%).
The values I designed are: VIN = 5V (4.7V to 5.45V), RFBT = 47K, RFBB = 10K, VOUT = 4.58V.
In this case, the duty cycle…
Part Number: TPS562207S Dear technical support,
I have a design where I would like to use the TPS562207S buck-converter.
The buck-converter is supposed to output 5 Volts and is being driven by a voltage source that can drop to as low as 6 Volts. From…
Part Number: TPS562207
Hello, My customer is facing long lead time issue about TPS562207. They can get TPS562207S instead somehow.
At current their design, can they just replace TPS562207 by TPS562207S with no modifications and with…