Part Number: TPS562207S Other Parts Discussed in Thread: TPS62122 , , TPS62901 , LM2621 Hi,
using TPS 62122 quite a while in an application, where VIN might vary from 2V - 12V, required VOUT is 2.3 - 3.6V - or whatever VIN does deliver (pass through); current…
Thanks Shuai, I'll try changing the polarity of the capacitor. I've ordered some sample of the TPS562207 which has a smaller layout than TPS564201 and the TPS564208. Where in the data sheet does the TPS564208 suggest it is FCCM? I see one line mentioning…
Part Number: TPS562202 Other Parts Discussed in Thread: TPS562207 , TPS562207S Hi team,
My customer has a question regarding Webench support for the TPS5622x devices.
TPS562202
- has customization and simulation
- does not have Bode plot option
TPS56…
Part Number: TPS563207 Other Parts Discussed in Thread: TPS562207 Hi team,
My customer want to know if the TPS563207 and TPS562207 could replace the MPS MP1653 and MP1657. (Pin to Pin and Bom to Bom) I have a schematic file and I will check, can team help…
Other Parts Discussed in Thread: TPS62148 , TPS562207S , TPS62110 Hi,
I'd like to know the reason why the maximum output voltage of DCAP series or DCS Control Sw reg
are lower than that of common PWM Sw reg?
For example, the maximum input voltage of…
Hi David,
The test is no problem. In light loading TPS562202S goes into skip frequency mode to get higher efficiency. The frequency decreases a lot. Because there is no large loading. The ripple is the energy of one pulse. So it's a little larger.…
Hi chentsu,
TPS562201 is SOT236 package, MP1652 is SOT563 package. You can look at the TPS562207 and the TPS562231 .
TPS562201 has no need the R3. With it, TPS562201 will has stability issue. Without it, MP1652 will has stability issue. You can use R3=0…