Part Number: TPS563201 Other Parts Discussed in Thread: TPS564201 Hi, TI Support Team
The following requests have been received from customers.
- Request a specific value of VFB for each temperature.
- part name : TPS563201, TPS564201
Graphs exist on…
Part Number: TPS563201 Hi,
Good Day. I have a customer who is working with TPS563201. Please see below his query for your reference. Thank you very much.
TPS563201 Datasheet section "1 Features" states:
"• Output Voltage Range: 0.76 V to 7 V…
Part Number: TPS563201 We are using tps563201dcr, and there is a problem;
1) IC uses 12V input and 3.3V output; When the load meter is at 2.9a, its voltage output and load meter current are normal;
2) However, when the IC uses 5V input and 3.3V output…
Part Number: TPS563201 Hi Team,
My customer needs to learn if TPS563201DDCR is CUP structure (referring to active circuitry on the die underneath the bond pads) to recognize the material, please kindly help to provide the information.
Thanks.
Part Number: TPS563201 Dear team
Dose TI have those data of TPS563201DDCR?
1.Charge device model (CDM)
2. Machine model (MM).
3. ESD Human Body Model
Many thanks
Denny
Part Number: TPS563201 Other Parts Discussed in Thread: TPS563208 Hi team,
My customer choose a Buck converter TPS563201, but they found a big current ripple in the light load due to the pulse skip mode.
So customer want to check if there are any ways…
Part Number: TPS563201 Other Parts Discussed in Thread: TPS563208 Hi Team,
There is a good new that we could DIN TI product! But cause TPS563201 is out of stock !
Could you help find out alternative solutions for the parts below? (can be supplied normally…
Part Number: TPS563201 Hi ti Team,
I have a project using TPS563201, and found that the voltage is as high as 0.81V at light load,This voltage has exceeded the specification range, as follows:
Part Number: TPS563201 Team,
my customer is using TPS563200DDC. Can they use TPS563201DDC as a pin-2-pin replacement?
The switching frequency is different. This probably needs different dimensioned external components. Will this also have impact on EMI? …
Part Number: TPS563201 Hi Experts,
TPS563201 over-current limit (OCL) is implemented using a cycle-by-cycle valley detect control circuit. But I find, when the valley current exceeds the threshold, there is no immediate protection, but action after a few…