Part Number: TPS563210A Tool/software: There is a mismatch in layout example pin number/order compared to pin configuration mentioned in datasheet
As per Pin Configuration
Pin 4 : PG
Pin 5 : SS
As per Layout Example
Pin 4 : SS
Pin 5 : PG…
Part Number: TPS563210A Other Parts Discussed in Thread: TPS62120 Hi Team,
I encountered an error while importing the PSPICE model of TPS563210A. Unfortunately after going through the creating new Macro this error appeared "Undefined parameter or possible…
Part Number: TPS563210A Hi team,
My customer would like to replace TPS563210A with TPS563210. Could we directly change IC without BOM changing?
Also, what is the difference between TPS563210A and TPS563210? There is a thread which mentions only different…
Part Number: TPS563210A We are running into an issue in our board where we are using LP87334D as PMIC and TPS563210 as pre regulator.
TPS563210 is giving high voltage and high ripple at no load. As per our design we know that it will go to Eco-Mode…
Part Number: TPS563210A Dear Sir,
I used TPS563210A to do a 5V input and 1V/0.3A ouput circuit. I found power-good signal is weird, please refer to following waveform, channel is output voltage and vhannel 2 is power-good signal.
Why there is a…
Part Number: TPS563210A Hi team,
Because PG-pin is open-drain, the following output appears after an external pull-up according to 7.3.3 Power Good.
1. When the output voltage is larger than 90% to the target value, the PG-pin become High.
2.…
Part Number: TPS563210A Hi team,
Could you please tell me the response time of OCL? If a over current occurs, how long will it take to limit the current?
Best, Zeming
Part Number: TPS563210A Other Parts Discussed in Thread: TPS563212 , TPS563211 Hi,
I check the datasheet that the device can support input voltage range is 4.5~17V.
My customer design requirement is input voltage 4.7V and output voltage 3.3V, inductor…
Part Number: TPS563210A Hi Team,
please provide datasheet for below MPNs
THE END CUSTOMER IS AVAGO TECHNOLOGIES.
TPS563210DDFR
TPS563210DDFT TPS563219DDFR TPS563219DDFT
Part Number: TPS563210A Hi team,
May I know what is high side FET VDS rating of TPS563210A? (VIN-VSW)
My customer is testing VDS for both high side and low side FET, we have VSW rating 19V max(DC) and 21V max(10ns transient), but I can not find…