Part Number: TPS563210A Hi team,
May I know what is high side FET VDS rating of TPS563210A? (VIN-VSW)
My customer is testing VDS for both high side and low side FET, we have VSW rating 19V max(DC) and 21V max(10ns transient), but I can not find…
Part Number: TPS563210A Hi team,
Please let me ask questions about EN-pin from customer.
1. Looking at Recommended Operating Conditions, it is OK to apply 17V to EN-pin. Is this true?
For example, is it OK to apply 15V to EN-pin when Vin = 12V…
Part Number: TPS563210A
Hi team,
Is there an upper limit on the capacitance of this external CSS for soft start?
Although they will use less than 0.47uF cap, they want to confirm the upper limit.
Regards,
Noriyuki Takahashi
Part Number: TPS563210A Other Parts Discussed in Thread: TPS563211 , TPS563212 Hello expert,
May I know if we have suitable device to replace MP1475? Thanks a lot!!
Best regards,
Ann Lien
Part Number: TPS563210A Hi team,
My customer use 1uH for output inductor on schematic. Our datasheet recommend the value is 1.5uH - 4.7uH.
What is the effect when they use 1uH inductor?
Vin = 8.5 - 17V
Vout = 1.8V
Iout = 2.1A
Best regards…
Part Number: TPS563210A Hi All,
I want to calculate the real OCP current, but the datasheet only provide the OCL part.
After checking the datasheet, the OCP current will be (IOCL + 1/2*ILripple).
But I wonder how the OCL current is measured? …
Part Number: TPS563210A Hi team,
I have a question about the soft start time.
My customer connected 0.047uF to SS-pin and expected 5.2ms soft start time(10% to 90% of Vout). However, the measured soft start time was 6.64ms. The variation of the 0…
Part Number: TPS563210A Hello,
Could you please help me to determine what the units should be for Css in the picture below?
I am hoping to determine what the soft start time will be for an 8.2nF capacitor.
Thanks,
Derek