Part Number: TPS563257 Tool/software: Hi,
We found peak voltage is too far away from the normal targat value during load transient. Using larger output capacitor can help it.
My question is what measurement should we care during a load transient test…
Part Number: TPS563257 Tool/software: Hi Team,
May I know what's item will affect the jitter cxcept for layout?
And I think BW will affect jitter since faster response then the frequency range will within a lower range compared with slower response…
Part Number: TPS563257 Hi Team,
May I know what's TPS563257 high side VDS absolute maximum voltage rating? In datasheet only have SW-GND rating.
I need both DC and Pulse, thank you.
Best Regards,
Roy
Part Number: TPS563257 Other Parts Discussed in Thread: DRV8220 Tool/software: Hi,
I'm thinking of using the TPS563257 for a design that needs variable voltage output between 0.6 and 9.5V from 12V input. I'd add resistors in parallel R5 (fig. 8-1…
Part Number: TPS563257 Hi Team,
Customer requested Fsw range SPEC. DS only provides TYP value. Could you kindly advise MIN and MAX value for Fsw?
TPS563257:
Thanks and best regards,
Terry
Part Number: TPS563257 Hi Team,
In TPS563257 datasheet it have SW-GND transient voltage spec as below. But I didn't see Vin-Vsw transient voltage spec? Could you let me know what's the Vin-Vsw transient voltage spec?
Best Regards,
Roy
Part Number: TPS563257 Hi,
For the circuit similar to the one mentioned in the datasheet of TPS563257 , I have connected 47k and 20k resistor (10nF is not connected) for the voltage divider to the enable pin. The supply voltage is steady 5V DC, the…
Part Number: TPS563257 Other Parts Discussed in Thread: TLV62568 HI team,
We plan to use TPS563257DRLR in our design but need to know more information on the PG pin which not mentioned in datasheet
1. What is the rated sink current for the PG pin…