Part Number: TPS56428 When the DC input of the TPS56428 is 12V, the output of the VREG5 exceeds 7V.
The circuit configuration was set identically to the EVM.
The output voltage is 3.3V, and the same symptoms are occurring on two PCBs.
If the VREG5…
Part Number: TPS56428 Tool/software: During IQA process, we found that the MSL indicated on the label of TPS56428RHLR does not match the MSL stated in the datasheet.
Could you confirm the correct MSL for this component and clarify if any changes have…
Part Number: TPS56428 The datasheet for this device specifies output capacitance values from 20-68uF. Are these values nominal values? Or are they referring to the effective capacitance values? Since these are high dielectric constant ceramic capacitors…
Part Number: TPS56428 Hi team,
Could you please let me know the minimum duty cycle of TPS56428?
My customer wants to use TPS56428 with VIN=12V and VOUT=0.7V, so he wants to know if it works properly and stable.
The datasheet mentions high duty…
Part Number: TPS56428 Other Parts Discussed in Thread: TPS54628 Hi,
I want someone to review the layout of TPS54628. I can share files offline.
Thanks
Tanveer
Part Number: TPS56428 For the dimensions of the thermal pad of the RHL (QFN) package variant of TPS56428, the datasheet page 25 reads, "THERMAL PAD: SIZE AND SHAPE SHOWN ON SEPARATE SHEET".
A: Can you please either tell us where the separate sheet is…
Part Number: TPS56428 Other Parts Discussed in Thread: TPS54325 Hi support team,
I have a question about the EN terminal of TPS54325 and TPS56428. Our customer is going to design using TPS54235 and TPS56428 now.
[Question] 1. How much is the hysteresis…
Part Number: TPS56428 Hi Experts, Good day. Our customer wants to know the below information, Please advise.
Please specify which (if any) of the below descriptions are applicable for part: TPS56428DDAR
(1) monolithic integrated circuits in which…
Part Number: TPS56428 Dear Sir,
The PG pin has been pull high to VREG on the datasheet.
I have one question need to check with you.
If the PG pin pull high to P3V3_AUX directly. Is there any question?
Part Number: TPS56428 Team,
can you please help to -
1. review their schematic for 2 instances of this device.
2. confirm their inductor selections are fine.
3. let me know if the inductors are overkill.
Device 1:
VIN = 12V
VOUT = 5…