Part Number: TPS56520 Hi team,
Is there an LTSPICE model of the TPS56520? I get a "Too few nodes" error when using the model on the web and cannot run it. If you have a file that I can run, I would appreciate it if you could provide it to me.
Best…
Part Number: TPS56520 I want to use the TPS56520 to generate a 1.4v - 2.6v i2c-programmable range. The "Application Report SLVA886–April 2017 A Practical Approach to Higher Output Voltage Applications for I2C Based DC/DC Converters" shows the schematic…
Part Number: TPS56520 Hi,
I have two questions about I2C SCL rate for TPS56520.
1. What is the I2C SCL default mode for TPS56520? Standard mode (100khz)?
2. Is there a option to change the mode from the standard mode to fast mode (400khz)?
Thanks…
Part Number: TPS56520 Hi Team,
When I look at the 7.6 Timing Requirements of datasheet of TPS56520 , tHD;DAT (Data Hold Time) says that Min=50ns and Max=900ns.
But when I look at the tHD;DAT specification of I2CBus user manual from NXP (Philips…
Part Number: TPS56520 Hi Team,
When I look at the 7.6 Timing Requirements of datasheet of TPS56520, tHD;DAT (Data Hold Time) says that Min=50ns and Max=900ns. But when I look at the tHD;DAT specification of I2CBus user manual from NXP (Philips), it…
Part Number: TPS56520
Hi,
Could you tell me the time from the device enable to the beginning of the start-up and the time from the enable to the rise of power-good?
Best Regards, Yuto Sakai
Other Parts Discussed in Thread: TPS56520 On the TPS56520 datasheet P.25, there is recommended capacitor value 44uF to 100uF. What value can we increase output capacitor value up to? Finally we ask our customer to confirm operation with their board, thus…