Part Number: TPS54302 Other Parts Discussed in Thread: TPS565201 Hi,
Obviously lots of sourcing issues right now, trying to find an available replacement for the TPS54302 . I looked through all of the TSOT-23-5 packages that I could use and it seems like…
Part Number: TPS565201 Hi team,
My customer is developing TPS565201. To improve the load transient response, they want to add a very large value Cout(hundreds of uF) at TPS565201output. So I just want to check with you is there any restriction on TPS565201…
Part Number: TPS565201 Other Parts Discussed in Thread: TPS565208 , Dear,
Here we met audio noise issue caused by inductor under light load condition. Attached file is the schematic and the spec for inductor. I guess that the noise is caused by Pulse Skip…
Part Number: TPS565201 When tps5655201 was started, there were two starts with an interval of 160ms. During the test, it was found that there was an over-current of 10us, and the current reached 6A
1、10us 6A过流是否会导致过流保护?
1. Does 10us 6A over-current lead…
Part Number: TPS565201 This is a question about the EN pin of TPS565201.
The difference between the input voltage of VIN and EN is not described in the data sheet.
Are you concerned about connecting VIN directly to ENpin?
Is it preferable to go through…
Part Number: TPS565201 Other Parts Discussed in Thread: TPS56528 Hi,
According to the WEBENCH result, the inductor current ripple is about 34% at Vin=12V, Vout=5V, Iout=4A. Is it no problem or too high? I have also tried to simulate with TPS56528, but…
Part Number: TPS565201 Hi,
I am designing a 7V-16V Vin to 5.1V Vout @ 3.5A regulator based on the TPS565201. There is a second power source in the design that may be occasionally connected. It would supply 5V at the output of the TPS565201. Is the TPS565201…
Part Number: TPS565201 Hello,
I wan to use this part to supply 5 A of current at 5 V.
What is the least Vin I can use to do this using this part, and what would the efficiency of the part be at that voltage?
Part Number: TPS565201 I am currently looking for some IBIS models to perform some power integrity (PI-AC) analisys through na electromagnetic simulation software. However, the software I use accepts ONLY the IBIS model of the components. Unfortunately…