Part Number: TPS565208 Abnormal voltage fluctuations on the VFB EN and VIN pins during power-up of the TPS565208.docx
During the TSP565208 tests on multiple models, it was found that the input pin, feedback pin, and enable pin all exhibited significant…
Part Number: TPS565208 Hi team,
some question during design need your help to confirm:
1.When VOUT=0.9V, the datasheet recommend to put the inductor value to be 1uH~4.7uH. is it acceptable to use 1uH? will there be stability risk cause the 1uH is…
Part Number: TPS565208 Hi team,
we suggest 20-68uF for Cout. will using a larger capacitor like 470uF lead to any risk?
any test recommended to add to prove the system is OK?
Part Number: TPS565208 Hey Team!
Working with this PSPICE model and running some output ripple tests. I noticed that the frequency of waves of the switch node is off. Instead of being ~526kHz, it's ~5/6MHz:
Part Number: TPS565208 Hi,
I have been working trying to get a bode plot for the loop gain out of PSPICE and I can't seem to get anywhere. Below is an image of my schematic
When I do an AC simulation, I get the following output
At first, this…
Part Number: TPS565208 Other Parts Discussed in Thread: TPS565201 So I was simulating the efficiency of this chip in pSPICE and one of the factors I was testing against was load. I know that some of these chips have light load efficiency, so I wanted…