Part Number: TPS565208 Other Parts Discussed in Thread: TINA-TI Good evening,
I am trying to export a WEBENCH design to TINA TI but the process has failed multiple times. I have also tried restarting the WEBENCH designer and recustomizing my circuit, but…
Part Number: TPS565208 Hi Support team
my customer is doing over voltage protection, the test method is short the FB PIN to GND,
after the testing, the controller will shut down and latch off,
may I know any idea to modify the over voltage protection…
Part Number: TPS565208 Hi Support team
pls refer following for TPS565208 application schematic
we suffered the start up issue both in max load no load conditions
in max load VOUT will have negative voltage
in no load VOUT will delay around 10mS after…
Part Number: TPS565208 Hi There,
Please find below the schematic. When the output voltage is tested without load, we get 2.5V RMS, but when loaded, the voltage drops down.
The below image is when the output is open:
The below screenshot is when the…
Part Number: TPS565208 Please let me know below condition.
Q1) Td TYP and MAX value
Q2) Any change by VOUT setting? What if VOUTMAX7V *0.9 case v.s VOUT 0.76V *1.1 Case? Tss: Datasheet typ 1.0ms,
Part Number: TPS565208
According to Datasheet , this diagram above is typical app.
I feel confused for R3(10kΩ) which is cast between EN-Signal and EN-pin.
I have two questions:
1. on dataSheet Pin Description Page.3 . for EN-pin it says : "Enable…
Part Number: TPS565208 Hello
We are using TPS565208 module to generate diff voltages like 3.3V, 1.2V, 1V from 5V.
We are doing QM333 on our product and we have faced that during the hot cycle the module has gone bad.
PFA schematic for reference.
Also…
Part Number: TPS565208 Hi all,
I am currently running into an issue with the TPS565208 Transient model available on PSPICE where the simulation for a load transient event does not continue to run after 33%. This also coincides with the middle of the…
Part Number: TPS565208 Hi Team,
I am using the TPS565208 in one of my products.
I have encountered with a problem. I’ve configured the component for a 6.1V output voltage, but for some reason I’m getting 2.5V .
Please see my schematics below…