Part Number: TPS566231
Hello
I'm using the TPS566231RQFR in a circuit to power a MCU and LED's. During bring-up, there is a problem with this regulator. (No load applied to the output yet, expect MCU with no Software in it yet)
There is the Problem…
Part Number: TPS566231 Hi,
is their any details available for Auto-skip mode for TPS566231PRQFR?
why to choose the same?
How it operates?
How to improvise the power dissipation?
How to increase thermal stability in contineous load operation…
Part Number: TPS566231 Tool/software: Hi Team,
I have attached the schematics captured with the parts TPS566231RQFR and TLV803EA26DPWR for the review.
Kindly go through and provide your feedback.
Thank you,
Manikandan R
Part Number: TPS566231 Tool/software: Hi Team,
I want to connect the EN pin to the microcontroller of 1.8V. But I want the internal pullup resistor value and the voltage it is pulled up, so i can decide whether i can connect the EN to microcontroller…
Part Number: TPS566231 Tool/software: Hi, I'm running into an issue with the TPS566231RQFR where about 10% of the time, it shorts VIN to GND upon the first power up. This has been an issue with various load connected as well as with all load disconnected…
Part Number: TPS566231 Hi team,
The EN pin is connected to weak pull up resistor.
What value pull down resistor is recommended to connect to make sure disable the device?
Regards,
Shoo
Part Number: TPS566231 Hi,
Does TI have Input 12V to output 5V/3A buck regulator with auto recover after OCP or OVP?
As I know must regulator will lockout when fault happen likes OCP or OVP, does TI have this kind of part can a uto recover and no…
Part Number: TPS566231 Hi,
We are using the device P/N : TPS566231PRQFR to realization below DC-DC Buck conversion
Vin : 3.3Vdc
Vout : 1.24V/2A
Ripple and Noise : 30mv pk-pk (maximum)
Operating Temperature : -40DegC to +85DegC
We have tested…
Part Number: TPS566231 I can do Startup Simulation and Steadystate Simulation of TPS566231P with slum773a, but can I do Simulation of Load Transient with PSpice for TI? If you can, please tell me how to do it.