Part Number: TPS56837H Tool/software: Hi team,
My customer is considering using a buck converter with the following specifications:
Input voltage range: 22.8 to 25.2V
Output voltage: 21.5V
Output current: 7A
Switching frequency: 300kHz or…
Part Number: TPS56837H Other Parts Discussed in Thread: TPS56837 Tool/software: Hi.
I encountered an issue when I adopted TPS56837H to build an USB-PD board.
Vin = 22.5Vdc, Vout = 5V, 9V, 15V, 20Vdc, max output power = 65W. Other components are the…
Part Number: TPS56837H Other Parts Discussed in Thread: TPS56837 Hello,
As a part of a power charging board I'm designing now I need to use the TPS56837H for converting 24v to 15v. .
Till now I considered working with TPS56837H since its data-sheet…
Part Number: TPS56837H Other Parts Discussed in Thread: TPS56837EVM , TPS56837 , Tool/software: Hi:
I used the TPS56837H chip to build a 24V to 12V step-down circuit, and the measured SW was more obvious than the overshoot, exceeding the SW pin withstand…
Part Number: TPS56837H Other Parts Discussed in Thread: LM3489 Tool/software: Hi,
what is the max. output voltage that can be achieved with the TPS56837H if it will be powered from the 19V notebook power supply? Advertised is 98% duty cycle supported…
Part Number: TPS56837H Tool/software: Hello,
It is not clear from datasheet why were the R1,R2 resistors of the Vin voltage divider for the V-UVLO were chosen to be : R1=169k, R2=36.1k ?
How these values support Vin=16v to 28v while UVLO voltage…
Part Number: TPS51388 Other Parts Discussed in Thread: TPS56837H Tool/software: Hello:
The current customer requires a synchronous switch buck converter that supports multiple output fast charging protocols, supports USB-C interface, PD3.1/PPS protocol…
Part Number: TPS56837H Good afternoon, I made a circuit using the CI texas TPS56837H for testing and evaluation, but I couldn't get the IC to work properly as expected. when feeding the IC with a low voltage (6 to 10 V) the output is activated and regulated…
Hi Mark
I didn't find the max duty in the datasheet neither. But the Webench should be trust-worthy.
Will you consider TPS56837H or TPS56837HA ? There is an apps note about the UST-C application of TPS56837HA .
Thank you