Part Number: TPS56A37 Under normal operating conditions, a failure was observed in which the TPS56A37 developed a short circuit between VIN and GND.
The power source is a 24V adapter, and the load current is approximately 3A maximum at 4V during AP…
Part Number: TPS56A37 Hi TI team,
We are currently using TPS56A37 in our design.There is a MOSFET that connects the output rail to the downstream system.
When this load-side MOSFET turns on, a significant inrush current occurs at the TPS56A37 output…
Part Number: TPS56A37 When designing with Vin=11.4~12.6V, Vout=10V, Iout=4A, Temp=60℃, and High Efficiency Design, the Operating Values show a Frequency of 317.16kHz. I understand that the TPS56A37 is fixed at 500kHz, but I would like to confirm whether…
Part Number: TPS56A37 Hi
Initial testing passed, but the 1206 input/output capacitors and 10×10 mm inductor may be too large for the customer's design. Can these components be downsized
Thanks
Part Number: TPS56A37 I have built a circuit with the TPS56A37 and the datasheet states it has overtemperature protection and 30C hysteresis. I loaded the circuit to 8A and the TPS56A37 reached 150C and shut off, but after an hour at room temperature…
Part Number: TPS56A37 Other Parts Discussed in Thread: TPS54561 , LM76005 Tool/software: Hi Team,
I have an external 24 V power supply where my requirement for external supply varies from 18V to 35V.
Suggest me any buck part that that can have input…
Part Number: TPS56A37 Tool/software: When the PG terminal of the TPS56A37 rises, it shows the following waveform. Is it possible that the IC is the cause of the waveform shown below? (CH2: PGOOD, CH3: +5V)
The circuit diagram is as follows, with PG…
Part Number: TPS56A37 Tool/software: Hi,
We use the TPS56A37 for our buck design, and the input voltage is 24V, output voltage is 5V, the schematic as below:
Now we c apture waveform for the SW pin as below:
We modify the Cout to 47uF Ceramic…