Part Number: TPS56C231 Hi,
May I know there have 0.78V/9A and 0.78V/2A efficiceny data?
Our customer want check 0.78V/2A still have good efficiceny in FCCM mode.
Thanks!
Jeff
Part Number: TPS56C231 Hi there,
we're planning to use the TPS56C231 to supply ~11 A at 0.85 V with a switching frequency of 400 kHz. The datasheet and WEBENCH designer are sometimes contradictory to each other so I hope you can help clarify things…
Part Number: TPS56C231 Other Parts Discussed in Thread: TPS56628 , TPS566238 Tool/software: Hi,
We are currently planning to use TPS56C231 for new products. We have the following unknowns when designing the new product.
①
MODE Selection states to…
Part Number: TPS56C231 Tool/software: Hi team,
Can you please help calculate the Power Dissipation?
Vin
12V
Vout
3.3V
Designed DC/DC (LDO) Specification
TPS56C231
IoMax
5.441A
…
Part Number: TPS56C231 Other Parts Discussed in Thread: TPS56C215 Hi Team
if I use TPS56C231. which can't be designed Vin:6.2 V Vout 5.1 V Iout=7A.
However if I use TPS56C215 can work normally.
do you think the difference is normal? and…
Part Number: TPS56C231 Tool/software: HI,
I am currently working on a design that involves the TPS56C231LRNNR and TPS546D24ARVFR components, and I require specific mechanical data to proceed with heatsink mounting considerations. Could you please provide…
Part Number: TPS56C231 Tool/software: Hello team,
We are using TPS56C231RNNR buck converter IC for converting 12V to 5V at 8A. We are getting an output of 5.24V. When checked with an oscilloscope we are getting noise at feedback pin (pic attached below…
Part Number: TPS56C231 Dear Team,
Here is our board file and schematic of TPS56C231RNNR, could you please help to review it and let me know your comments?
U7749-240114-1.rar
Many Thanks,
Jimmy
Part Number: TPS56C231 Tool/software: Hi
I am using this Buck converter in my design, where Vin = 12V, Vout = 5V, Iout = 8A.
I m attaching pdf file of my design please suggest if any changes are required in this.
5va.pdf
Regards,
Nitesh M…
Part Number: TPS56C231 Tool/software: Hi Team,
is the PG pin coupled with the EN pin? If enable is pulled low will the PG be also low even if the output voltage is within the PG windows (above 93%)? This can make a difference in the power down sequence…