Part Number: TPS57160-Q1 Hi team,
In the datasheet,Equation 47 (Pg35) and equation 51(Pg36), how can we find the value of gm(ps) and gm(EV) to calculate?
on page 5, 7.5 Electrical Characteristics,Which value is gm(ps) or gm(EV)?
Another question,about…
Part Number: TPS57160-Q1 Hi, Team,
My customer need a formula to calculate the stop voltage, could you help support it? Thanks!
Their condition: 6.25V typ.(min: 5.95V) /450mA output, need to know the min input voltage.
Part Number: TPS57160-Q1 Hello,
I need unencrypted spice average model for TPS57160. I need to check the stability of the converter.
I also like to check the Middle-brook's criteria between the Pi-filter and Converter.
Please take up this topic at…
Part Number: TPS57160-Q1 Hello,
I am getting error,while importing Pspice model to LTspice. While creating symbol, It is showing " Unusually this is a Permission problem"
Kindly provide the solution.
Thank you,
Part Number: TPS57160-Q1 Hello Team,
I got some questions from our customer about TPS57160-Q1.
Q. Do you have variation data of Fsw at RT mode? Customer want to know the Fsw tolerance which is caused by TPS57160-Q1 part-to-part.
Q. Do you have variation…
Part Number: TPS57160-Q1 Hello Team,
I'm Yuta Kurimoto TIJ FAE.
Now Our customer is evaluating TPS57610-Q1. In their usecase, when the battery is connected reverse polarity, The VIN pin is exposed to -1.2V(10ms) instantaneously.
I know the abs max…
Part Number: TPS57160-Q1 Other Parts Discussed in Thread: TINA-TI Hi,
I have tried importing the PSpice model of TPS57160-Q1 into LTspice, since I had some problems simulating the device in Webench(see other posts). However, there is a problem with the…
Part Number: TPS57160-Q1 Hello,
I am trying to simulate the TPS57160-Q1 schematic in Pspice simulator. It is taking longtime and not finding the waveforms.
Kindly let me know, any initial parameters, I have to update in the simulation profile. If you…
Part Number: TPS57160-Q1 Other Parts Discussed in Thread: LMR36015 Hi team,
My client designs power supply based on TPS57160-Q1 with Vout=7V. During cold crank, the Vin can drop to 6V for 50ms. We need to configure the TPS57160-Q1 in such way that the…
Part Number: TPS57160-Q1 Hi, we have a new board built with TPS57160-Q1 for buck operation. In the initial test bypassed the input but directly applied 30V on the PH output (at the load side, so there is an inductor between the 30V and PH pin) to test…