Part Number: TPS61023 Other Parts Discussed in Thread: TPS631010 , TPS63001 , TPS631000 Tool/software: Hi, I designed a buck boost regulator based on this TPS61023DRLR. I am getting same output as input. Can someone help me to figure it out? Input = 5V…
Part Number: TPS61023 Other Parts Discussed in Thread: TPS60123 ,
Tool/software:
Hi,
I have a circuit using a TPD61023DRLR to generate 5V from two AA cells in series.
I'm testing the circuit using a poer supply varying the voltage to check operation…
Part Number: TPS61023 Hello,
Is there a inductor L1 value design method or value VS output current table for reference?
If I select a 2.2uH inductor, how much the rated output currrent?
Thanks.
Part Number: TPS61023 Tool/software: I am not able to find PSPICE model for TPS61023, I want to simulate it for my ongoing project. Please share the PSPICE model for TPS61023 with me at earliest. My requirements are-> Vin-3.3V and Vout-3.8V/2A.
Part Number: TPS61023 Other Parts Discussed in Thread: TPS61299 , TPS61021A Tool/software: Hello
I am trying to confirm the TPS61023 will actually start up when used with a 1.5V battery.
My project only has room for 11mm coin cell battery, which are…
Part Number: TPS61023 I recently purchased this chip and am struggling to determine where pin 1 is. I believe the orientation has something to do with the long strip on the left hand side, but I want to be sure before I proceed.
This is what it mentions…
Part Number: TPS61023 We made a following schematic. On giving Vin = 4V using battery, Vout was 5.06V as expected. Load is very light and should be in few mA. We are just powering MCU.
Now the Vout is at~ 1V. What could be caused ?
We didn't touch…
Part Number: TPS61023 Other Parts Discussed in Thread: TUSB320 Hello.
I am using TPS61023 in my design as Boost converter which can charge external devices. For the negotiation purposes I am using TUSB320 as Power Delivery. Basically I was following…
Part Number: TPS61023
I don't want to use EN pin. Can it be tied to Vin Pin so it is always in PU state when Vin is applied ?
if yes, Please also suggest suitable Resistance value between EN and Vin pin. Is 2kohm Enough ?
Thanks
Part Number: TPS61023 hi expert,
my customer will use TPS61023 in hot-swapped application and they are afraid that the voltage spike will damage the chip.
Does our device have hot-swapped application and do u have any advice ?
the customer also…