Part Number: TPS61025 Other Parts Discussed in Thread: TPS61299 Dear team,
I am looking for a newer drop in replacement for the TPS61025, which part would you recommend?
Thank you.
Kind regards,
Wouter Kragt
Part Number: TPS61025 Hi Team
Bought from Arrow and are seeing differences layout in lead frames for different assembly sites.
Please advise if this is normal and if it will affect its functionality, fit or form. Thanks!
Affected assembly site:…
Part Number: TPS61025 Hi,
I use TPS61025 to supply 3.3V to my product. For various technical reasons we ned to boost the internal rail to 3.6V. There is nothing connected to the FB pin. I know 61025 is not an adjustable version, but is there any way…
Part Number: TPS61025 Hi, Iam doing low power board design and just get ~1V output from TPS61025 VOUT pin. C3 is used low ESR Tantalum Capacitor - KEMET T520B107M006ATE040. Where can be issue ?
Schematic_ESP8266 low power board Sensor_2020-05-11_08…
Part Number: TPS61025 When disconnecting the load from this device, the device becomes unstable and starts consuming about 240mA. This happens about 20 percent of the time on my PCB even when the load is connected on powerup. Below is the circuit being…
Part Number: TPS61025 Dear TI Team
I would like to ask about capacitance of output capacitor.
Our customers are considering using it under the following conditions, and when Cmin was calculated using the following Cmin formula, Cmin was calculated…
Part Number: TPS61025 Other Parts Discussed in Thread: TPS61020EVM-025 I found that the part is causing substantial Vin noise on my implementation at most input voltages. I performed the same set of tests with the TPS61020EVM-025 and found mostly the…
sorry. we don't have this data as it is old part. i think we can use TPS61020 with same R3, R4 as the EVM to simulate the TPS61025.
Or Apply an EVM and replace the TPS61020 with TPS61025 for evaluation.
Part Number: TPS61025 Other Parts Discussed in Thread: TPS61201 , Hi, I am using the TPS61025EVM to power my design but saw a post by one of your engineers about possibly switching to another Boost Regulator because of tantalum cap. I saw this one and…
Part Number: TPS61025 Hello. I am using TPS61025DRCR - version 3.3V. Sometimes the microcircuit is turned on and supplies the output voltage from 4.8 to 5.0 V. The input voltage is 1.8V, the output current is not more than 50 mA. If raise the input voltage…