Part Number: TPS61027 Tool/software: Hello,
I want to confirm that the TPS61027DRCR and TPS61027DRCRSY have the same temperature range specification. According to the TI product page, they both have the same temperature spec which is -40°C to 125°C…
Part Number: TPS61027 Other Parts Discussed in Thread: TPS61020EVM-025 Tool/software: I am testing the TPS61027DRCR using the TPS61020EVM-025 evaluation board . The output is set to 5 V and the input supply is 3.3V When applying a load transient from…
Part Number: TPS61027 Other Parts Discussed in Thread: BQ25616 ,
Dear TI,
I would like to seek support from you regarding the use of the TPS61027 to power the BQ25616. The BQ25616 works properly when I power it from an external power supply. However…
Part Number: TPS61027 Other Parts Discussed in Thread: TPS61033 , TPS61022 Tool/software: Hi Team,
In my design, the input voltage (Vin) is fixed at 3.3V, and the output voltage (Vout) is set to 5V using the TPS61027DRCR boost converter. The load current…
Part Number: TPS61027 Other Parts Discussed in Thread: BQ25616EVM , , BQ25616 , TCA9548A , INA260 Dear TI, First of all, thank you very much for your technical supports, especially with my BQ25616EVM and TPS61020EVM. I was able to get the system to work…
Part Number: TPS61027 Dear TI Community,
I have a strange behavior from my TPS61027 and I appreciate if someone could give me a guide to fix this issue. I attached the schematics below:
In this schematic, please ignore JP2 as I short its connection…
Part Number: TPS61027 Other Parts Discussed in Thread: TPS61025 Dear TI,
First of all, thank you very much for your super supports Travis and Nini,. I would not be able to go this far without you.
I have tested the system with TPS61027 and I noticed…
Part Number: TPS61027 Hello,
I am using the TPS61027DRCR regulator to convert a 4-cell battery (3.6V to 6.5V) to 5V. When I start testing the PCB, I see a sudden increase in current because a short-circuit is produced between the input voltage (VBAT…
Part Number: TPS61027 Hello,
I would like to ask you about the TPS61027. Specifications are below. I am assuming that a motor will be connected to VOUT, but are there any concerns? Is it okay if the back electromotive force is applied to VOUT?
(Specification…
Part Number: BQ25616EVM Other Parts Discussed in Thread: TPS61027 , BQ25616 , TCA9548A , INA260 Dear TI, First of all, thank you very much for your technical supports, especially with my BQ25616EVM and TPS61020EVM. I was able to get the system to work…