Part Number: TPS61030 Hello,
my TPS61030 board generally working fine. (3.2V battery to 5V)
After some time of testing the board stops working, short between SW and GND.
I can not say exactly when it happens. My guess is that it happens i plug…
Part Number: TPS61032 Other Parts Discussed in Thread: TPS61030 Hi team,
I'm looking at using the TPS61032 as an alternate to the TPS61030 in the QFN package. Am I okay to place the TPS61032 on the board and leave the feedback resistors, that I had…
Part Number: TPS61030 Other Parts Discussed in Thread: TPS61022 Hi,
I read a document named Backup Power Solution Using Supercap with TPS61030 for Data Concentrator Circuit
http://www.ti.com/lit/ug/tidu594/tidu594.pdf
In the document, it says…
Part Number: TPS61030 Hi,
I read a document named Backup Power Solution Using Supercap with TPS61030 for Data Concentrator Circuit
http://www.ti.com/lit/ug/tidu594/tidu594.pdf
In the document, it says that:"As the real Vout =5V, Vout_re can be…
Part Number: TPS61030 Hi Sir
I used TPS61030PWPR, here is my circuit.
When I measured the output waveform, something wrong.
Red is output 5V and Blue is input 3.3V.
Why 5V has noise (distortion? drop?) and influence input 3.3V?
Would you…
Part Number: TPS61030 Other Parts Discussed in Thread: TPS61230 , TPS61230A Hello everybody,
We are using a TPS61030, as a power supply for our product (a calculator for off road vehicles). You can see our schematics attached to this post.
We are…
Hi Ibrahim,
In your real application, I suggest that you put battery near to TPS61030 and make sure the trace connecting them is wide enough. So the resistance between battery and TPS61030 is very small and the voltage drop on it is ignorable. So only…
Part Number: TPS61030 Can you please describe the behavior of the TPS61030 under the following two conditions.
Condition 1: TPS61030 Vout =3.8V, VBAT input = 2.7V, output is ENABLED (EN =VBAT)
What would occur if the TPS61030 output is driven by another…
We have Bypassed everything before TPS61030 and connected battery to the VBAT of it. And still getting sound like TICK TICK TICK........
Moreover we have solved the problem of continuous beep from it by changing output capacitor 220uF from ceramic…