Part Number: TPS61032 Our customers are currently considering using the TPS61032 and I have been asked by them to confirm the schematic.
If you check their schematics, the inductor is 2.7μH. However, based on the conditions used by the customer (shown…
Part Number: TPS61032 Other Parts Discussed in Thread: TPS61023 , TPS61230A Hi,
I am using TPS61032 IC which doesn't require external resistors since output voltage is fixed. What do you suggest me to do with this pin? I am not willing to leave it floating…
Part Number: TPS61032 Hi,
I recently posted question forum about behavior of following schematic, I changed PCB footprint, but issue persisted (low voltage on output and high consumption on empty load).
Input voltage was 2.4V, output voltage was 1…
Part Number: TPS61032 We have a PCB circuit design that uses TPS61032.
Designed output is 5V/1A for two output loadings. 1st loading is 5V/400mA, 2nd loading is 5V/200mA. This is for a 3 stage switch (0,1,2) power supply system. SW1=0, All off; SW1…
Part Number: TPS61032 We are using the TPS61032 with a supercap charging circuit to make steady-state 5.25V for a modem that requires extremely stable voltage. Everything works fine 99% of the time but I have had 10 intermittent failures and every time…
Part Number: TPS61032 Other Parts Discussed in Thread: TPS61030 , TPS61235P , TPS61236P Hello,
I am trying to create a battery backup system for a raspberry pi model 3. We are creating a player for digital signage application and knowing common issues…
Part Number: TPS61032 Hi,
Hi, I having problem with power supply, which for inputs from 1.8 - 2.8 V from battery should generate 5V on output. Currently I don't have load on output, I just measured voltage there, which was around 1.5V and circuit TPS61032RSAR…
Part Number: TPS61032 Other Parts Discussed in Thread: TPS61230 Hello,
I need help for the TPS61032 output issue. Our purpose is to get a 5V output with a 4.5V input. The maximum current that we need on the output is 1.6A. To do it, we use a 4.7uH…