Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: WEBENCH-POWER-DESIGNER Other Parts Discussed in Thread: TPS61033 Hi support team,
It seems that TPS61033 does not support WEBENCH. Do you know the support schedule?
Regards, Dice-K
Part Number: TPS61033 Hi support team,
Is it possible to switch the MODE pin high/low during operation to switch to FPWM or Auto PFM? Will VOUT be temporarily interrupted?
Regards, Dice-K
Part Number: TPS61033 Hi support team, This is a question regarding PFM operation.
Is there a way to calculate the waveform and frequency of PFM under the following conditions?
VIN = 5.3V VOUT= 5.5V IOUT= 0.05A L = 2.2μH
Is it best to check by experiment…
Part Number: TPS61033 Other Parts Discussed in Thread: TPS61023 , TLV61070A , TPS61020
Hi support team, I would like to calculate IOUT to shift to PFM.
Does it shift to PFM when the inductor valley current is 0A?
Calculating with the following conditions…
Part Number: TPS61033 Hi support team, This is a question when using the MODE pin fixed at High.
Is it okay to connect the MODE pin and VIN pin directly? This is a confirmation because there is no description for ABS and ROC. According to TPS61033EVM-105…
Part Number: TPS61033 Hi support team, This is a question regarding the operation when returning from pass-through mode with MODE=Low setting.
When VIN drops and VOUT becomes less than 97% of the setting target voltage, does it always recover with PWM…
Part Number: TPS61033 TPS610993, an output voltage of 3.0V should be obtained with an input voltage of 0.7V~5.5V, but in the following circuit configuration, the output voltage becomes 5.5V in rare cases when VBAT is turned on.(The schematic will be uploaded…
Part Number: TPS61033 Other Parts Discussed in Thread: BQ24610 , TPS61376 Hello guys,
One of my customers is looking for a DCDC boost converter IC which has VINDCM(Input Voltage Dynamic Power Management) function.
The customer wants to build a product…
Part Number: TPS61033 Other Parts Discussed in Thread: TPS2116 , TPS61022 , TPS2117 , , , TPS63802
Hello,
I designed a circuit with 2 voltage sources, one of them TPS61022, followed by a multiplexer TPS2116. This obviously was a mistake, because a short…