Part Number: TLV61048 Other Parts Discussed in Thread: TPS63070 , TPS61033 Tool/software: Hi team,
I have three question about this product.
①In datasheet figure 1, it is said VBAT is Powe Stage Input. In my understanding VBAT is bias input voltage…
Part Number: TPS61240-Q1 Other Parts Discussed in Thread: TPS61240 , TPS61033 Hello Team,
Our customer want to confirm the loop response at fixed output device.
As far as I confirmed FB pin is just connected to the top of internal resistor divider…
Part Number: TPS61376 Other Parts Discussed in Thread: TPS61033 , TPS60133 Dear,
I am working on a design and was wondering how I can easily calculate the compensation network? Is there some tool for this? Or is there a simulator for this?
The design…
Part Number: TPS61033EVM Other Parts Discussed in Thread: TPS61033 we have this dev kit.
Test 1.
The input voltage is 3V/2Amp
Output voltage is set to 5V.
Test 2.
The input voltage is 4V/2Amp
Output voltage is set to 5V.
we are running…
Part Number: TPS61088 Other Parts Discussed in Thread: TPS61033 Tool/software: Hello TI Support,
We are using the TPS61088RHLR as a boost regulator to generate 4.5 V from a Li-ion battery (VBAT 3.0–4.2 V). With EN driven low, we expect the output to…
Part Number: TPS61202 Other Parts Discussed in Thread: TPS61033 , TPS61299 We are trying to build a boost circuit using your product TPS61202.
Can the TPS61202 operate in parallel?
Part Number: BQ25890 Other Parts Discussed in Thread: TPS61033 , BQ25638 Dear TI Teams,
We have a new project that requires the use of a charging IC, which needs to charging the 1-cell 5000mAH Li-Lon battery and also output 5V/2A to the system load…
Part Number: TPS61033EVM Other Parts Discussed in Thread: TPS61033 , , BQ25790EVM , BQ25790 Hi ,
We are developing a Handheld device and Processor Board requirement is 5V @700mA.
We plan to use following design as below.
We have selected 9000mAH…
Part Number: TPS63900 Other Parts Discussed in Thread: TPS61094 , TPS61033 , TPS61022
Tool/software:
Good morning,
I am working on a design of a NB-IOT product with a bobbin battery (LI-SOCL2) + ELDC supercapacitor (1.5F) Vin = 2.5 - 3.8V Vout NB…
Part Number: TPS61022 Other Parts Discussed in Thread: TPS61033 , Hi team,
About TPS61022 and TPS61033, could you let me know if reverse current flows from Vout to Vin when shutdown mode (EN=L)?
The datasheet mentions that during shutdown, the load…